跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

TPS-1 PROFINET Stack and Updated GSDML Files

Last Updated:06/01/2017

Question:

Does the GSDML file change as the TPS is updated?

Answer:

Every version of the TPS-1 development toolkit comes with a set of GSDML files that reflect the feature set implemented in the current PROFINET stack. These files comply with the requirements of the current PROFINET and GSDML specifications.
Suitable Products
TPS-1
  • 这篇文章对您有帮助吗?