跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Max CPU Speed of TPS-1

Last Updated:06/01/2017

Question:

What is the maximum speed of the CPU in the TPS-1?

Answer:

The maximum operating frequency of the internal CPU is 100MHz.
Suitable Products
TPS-1