跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

IP Address of TPS-1 Set and Retrieved by Host MCU

Last Updated:06/01/2017

Question:

Can you get and set the IP address of TPS-1 by the host MCU?

Answer:

Yes, the driver software includes the APIs to both get and set the IP address.  Please refer to the APIs TPS_GetIPConfig and SetIPConfig in the TPS-1 toolkit driver manual.
Suitable Products
TPS-1