跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

For the UPD98431, how long is the mirror port I/O delay time?

Latest Updated:08/01/2005

Question:

For the UPD98431, how long is the mirror port I/O delay time?

Answer:

This delay time, which depends on the clock deviation of the internal synchronization circuit, is in the range of 0 to 8 clocks.
Suitable Products
I/F for Serial Control