跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

sf_audio_record_adc Module Guide Resources

Last Updated:08/03/2017

Question:

Where can I find the references to module guide resources for the Module module on module?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Under Construction

Will be updated when the module guide is published.

Suitable Products
SSP 1.2.0 and above
  • 这篇文章对您有帮助吗?