跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

r_doc Module Guide Resources

Latest Updated:11/27/2017

Question:

What resources are available for the r_doc module?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The Data Operation Circuit (DOC) HAL module is a high-level API for DOC applications and is implemented on r_doc. The DOC HAL module uses the DOC peripherals on the Renesas Synergy™ MCU device. A user-defined callback can be created to inform the CPU when an event occurs.

The DOC HAL module peripheral is used to compare 16-bit data and can detect the following events:

  • A mismatch or match between data values
  • Overflow of an addition operation
  • Underflow of a subtraction operation

Module Guide

The DOC HAL module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the DOC HAL module guide application note, application project and import guide are available here

Module Guide Resources

  • Content provided as it becomes available.

Known Issues

  • For all known issues refer to the most recent SSP release notes for known issues located here.

 

SSP
  • 这篇文章对您有帮助吗?