跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Why is the SSP license file selection button missing from the preferences window?

Last Updated:04/04/2017

Question:

Why can't I see the SSP license file selection button on my preferences window?

Answer:

If the screen resolution is set too high the right side of some windows, like the license file preference window, can be cut off.

Pref.jpg.

Solutions to this issue are: For Windows 7: Change the setting of the item size to the default as illustrated in the below figure.

ButtonFig2.jpg

Or, execute e2 studio using the XP Compatible mode with "Disable display scaling on high DPI settings" deselected as shown below.

ButtonFig3.png

For Windows 10: Lower the font size of Title bars, Menus and Message boxes by going to Control Panel > Appearance and Personalization > Display > Make text and other items larger or smaller.

ButtonFig4.png

Suitable Products
SSP and e2 studio