跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the current SSP revision and when is the next release scheduled?

Latest Updated:10/13/2016

Question:

What is the current SSP revision and when is the next scheduled release?

Answer:

The current revision of SSP is 1.1.3 and the next release, 1.2.0-beta is scheduled for the beginning of Nov 2016.
Suitable Products
SSP
  • 这篇文章对您有帮助吗?