跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the Renesas Flash programming tool?

Latest Updated:10/24/2016

Question:

What is the RFP tool?

Answer:

The RFP tool is used to program over the Flash segment that holds the factory installed boot program. Users can install their own boot program using this tool. You can find out more about this tool here: https://www.renesas.com/doc/pr...ej0100-rfp.pdf
Suitable Products
SSP