跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What can I do if I'm seeing excessive build times on my Synergy Project?

Latest Updated:10/11/2016

Question:

I'm seeing excessive build times on my Synergy project. What can I do to reduce these build times?

Answer:

One possibility for improving build time is to make sure the project isn't recompiling portions of the project unnecessarily. For example, if the project is recompiling all files, even if n o source files have changed, this may be due to an incorrect refresh policy. You can check this by going to the project settings, C/C++ Build and then to the Refresh Policy tab. The resource on the tab should be the folder name for the project. This might not have been changed if the project was moved from another location. Remove any incorrect resource and add the correct folder location.Clean and Build the project. It should process quicker in subsequent builds when code is unchanged.

 

  • 这篇文章对您有帮助吗?