跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Using Event Flags FAQ

Last Updated: 10/07/2015

What are Event Flags?

Event flags provide a powerful tool for thread synchronization. Each event flag is represented by a single bit. Event flags are arranged in groups of 32.

How do Event Flags work?

Threads can operate on all 32 event flags in a group at the same time. Events are set by tx_event_flags_set and are retrieved by tx_event_flags_get.
Setting event flags is done with a logical AND/OR operation between the current event flags and the new event flags. The type of logical operation (either an AND or OR) is specified in the tx_event_flags_set call.
There are similar logical options for retrieval of event flags. A get request can specify that all specified event flags are required (a logical AND). Alternatively, a get request can specify that any of the specified event flags will satisfy the request (a logical OR). The type of logical operation associated with event flags retrieval is specified in the tx_event_flags_get call.

How are Event Flags created?

Event flags groups are created either during initialization or during run-time by application threads. At the time of their creation, all event flags in the group are set to zero. There is no limit on the number of event flags groups in an application.

What happens when a thread wants to get from Event Flags?

Application threads can suspend while attempting to get any logical combination of event flags from a group. After an event flag is set, the get requests of all suspended threads are reviewed. All the threads that now have the required event flags are resumed.
All suspended threads on an event flags group are reviewed when its event flags are set. This, of course, introduces additional overhead. Therefore, it is good practice to limit the number of threads using the same event flags group to a reasonable number.

How can notifications be used with Event Flags?

Some applications may find it advantageous to be notified whenever an event flag is set. ThreadX provides this ability through the tx_event_flags_set_notify service. This service registers the supplied application notification function with the specified event flags group. ThreadX will subsequently invoke this application notification function whenever an event flag in the group is set. The exact processing within the application notification function is determined by the application, but it typically consists of resuming the appropriate thread for processing the new event flag.

Where can I find more information?

You can find more information on the ThreadX user manual, available here

 

©1997-2015 by Express Logic, Inc. All rights reserved. This document and the associated ThreadX software are the sole property of Express Logic, Inc. Each contains proprietary information of Express Logic, Inc.

  • 这篇文章对您有帮助吗?