跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Synergy Suggestion Box

Latest Updated:10/04/2016

Question:

How do I leave feedback or suggestions on the various elements of the Synergy Platform?

 

Answer:

You can leave feedback on any Synergy Platform elements or the Synergy Support system by simply clicking on the Leave Feedback button at at bottom of this article. Note that this button is at the bottom of EVERY article in the Knowledge Base so you can also leave feedback on a particular article by clicking on the corresponding button. You can also vote on the helpfulness of a particular article by giving a Yes or NO vote at the bottom of an article. This vote helps place the article in terms of relevance during a search and also provides feedback to the article author so they can improve the articles helpfulness.

 

  • 这篇文章对您有帮助吗?