跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

SSP Version 1.4.0 Usage Notes

Last Updated:03/30/2018

SSP Version 1.4.0 usage notes can be found in the attached PDF.

The usage notes include issues and workarounds for BSP, HAL, Framework, and Express Logic modules, as well as MCU implementation/SW architecture.

sspv140-v101_Additional-Usage-Notes.pdf

 

  • 这篇文章对您有帮助吗?