跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

SSP 1.3.2 Release- Additional Information

Last Updated:12/05/2017

Question:

Where can I find additional information related to the SSP 1.3.2 release?

Answer:

You can find additional information on the SSP 1.3.2 release on this page. In particular, a document showing additional issues related to the SSP 1.3.2 release is available here. These augment the issues described in the published release notes on the Synergy Gallery.
Suitable Products
SSP
  • 这篇文章对您有帮助吗?