跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Reference Template

Details

Offer the details a user needs to know about the definition, parameters, and so on. Tables are extremely useful for looking up information and organizing the details that readers want to know.

Definition

void print(String message)

Parameters

message
Type: String
Message to print.

Response

Upon successful invocation, this feature returns ...

Exceptions

Exception Condition
ArgumentNullException message is null.
   

Remarks

Additional points to consider are ...

Examples

Example 1:

First example shows ...

Example 2:

Second example shows ...

Considerations

Give some considerations such as system requirements or "gotchas" for this setting or control or programming syntax.

  • 这篇文章对您有帮助吗?