跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

NetX Telnet Server Module Guide Resources

Last Updated:01/10/2018

Question:

Where can I find the resources for the NetX Telnet Server Module Guide?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The Telnet Protocol (Telnet) is a protocol designed for transferring commands and responses between two nodes on the internet. Telnet is a simple protocol that utilizes reliable Transmission Control Protocol (TCP) services to perform its transfer function. Because of this, Telnet is a highly reliable transfer protocol. Telnet is also one of the most used application protocols.

The NetX Telnet Server module supports the following features:

  • The NetX Telnet Server module is compliant with RFC854 and related RFCs.
  • Provides high-level APIs to:
    • Support multi-thread operation
    • Support callbacks for common functions
      • Authentication
      • New Connection
      • Receive Data
      • End Connection
    • Support some Option negotiation
      • Echo
      • Suppress Go Ahead

Module Guide

The NetX Telnet Server module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the NetX Telnet module guide application note, application project and import guide are available here.

Module Guide Resources

The following application projects are available from the Renesas web site at the referenced url.

  • NetX Telnet Client Module Guide - Application Project here.
  • NetX Port Ether Module Guide - Application Project here.

To find out more about the details of operation refer to the NetX Telnet User's Manual, part of the X-Ware Documentation zip file located on the Synergy Gallery here.

Known issues

  • Refer to the SSP release notes for known issues, available here.
Suitable Products
SSP
  • 这篇文章对您有帮助吗?