跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is wear leveling for external QSPI memories supported within SSP 1.1.1?

Latest Updated:10/04/2016

Question:

Is wear leveling supported in SSP 1.1.1 for external QSPI Flash memories?

Answer:

Wear leveling is not supported for QSPI Flash devices as of SSP 1.1.1. Check current release notes and the SSP Users Guide to see if it is supported in future releases.
  • 这篇文章对您有帮助吗?