跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

IBIS Models for Synergy MCUs

Latest Updated:10/04/2016

Question:

Where can I get IBIS files for Synergy MCUs?

Answer:

IBIS models for Synergy S7G2 MCUs are available now for both 3.0 and 3.3V systems. These files are attached to this article below. You can also find IBIS models in the Downloads Tab on the Synergy MCU web page. Foe example- this is the location for the IBIS models for the S7G2.

https://www.renesas.com/en-us/produc...7-series.html#

Note that you can select IBIS/BSDL to search for these file types.

  • 这篇文章对您有帮助吗?