跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How will Renesas add new ThreadX releases to the Synergy Platform?

Latest Updated:10/04/2016

Question:

ThreadX will be making periodic updates to their code. How will Renesas add new ThreadX releases to the Synergy Platform?.

Answer:

The Synergy Platform uses the mainstream Express Logic release. Should there be an update to ThreadX we plan to follow with our normal testing and release schedules. The current Synergy Platform release schedule calls for a major release every 6 months, minor releases every 3 months and periodic bug fixes on an as needed basis.

  • 这篇文章对您有帮助吗?