跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How to install all the development tools used with the Renesas Synergy Platform

Last Updated:03/22/2018

Goal

After completing this how-to you will be ready to use all the software tools needed to develop with the Synergy Software Platform.

An Overview of Downloading and Installing Synergy Platform Tools

There are two different ISDEs available for developing with the Synergy Platform. The Renesas e2 studio ISDE is an eclipse based development environment and leverages the familiar GCC tool flow. The IAR Engineering Workbench for Renesas Synergy (IAR EW for Synergy) is also available and provides the familiar IAR tool flow. Developers can select either of these environments based on their experience and development needs. Both of these advanced ISDE's are available free of charge. 

Installing either ISDE has been simplified over previous installation processes now that the Platform Installers are available. The Platform installer will install all the components needed for the ISDE in one simple step. The remainder of this how to article will guide you through these steps so that you end up with the ISDE you want to use in your development environment.

Note: An article showing the previous version of the installation process is available if you need to install a previous version of an ISDE not supported by a Platform Installer. You can find that article here: Click Here

1: Download the Platform Installer for Your ISDE

You will need to download the Platform Installer associated with the ISDE you wish to use for your Synergy development projects. This step well guide you through the process of downloading the files you will need depending on your target ISDE. 
 
If you want to install the e2 studio based ISDE:
  • Navigate to the SSP page on the Renesas Website. Find the Download section. If you are not already signed in to MyRenesas clicking on the Download button will bring up the MyRenesas login window. Login and you should come back to the SSP web page. The Download button should now show as Download Platform Installer. Click that button and select the e2studio option. The download will begin. This is a big file since it includes everything. The download will take several minutes.

If you want to install the IAR-based ISDE:

  • Follow the above steps but select the IAR option in the Platform Installer selection window. The download will begin. This is a big file since it includes everything. The download will take several minutes.

2: Install the ISDE 

After downloading the tool, it is time to install it. Move the downloaded set-up file to your computer desktop, open it, and follow the installation instructions. Note that the below screenshots are for SSP 1.3.2. The screen shots are very similar for later versions, just the revision numbers have been changed.

2.1: Install the e2 studio based ISDE

To install the e2 studio based ISDE, open the e2 studio installer.  Click Yes on the Confirmation window. This will begin the Extraction Process.
 
Install_Confirm.PNG  Extracting.PNG
 
Figure 3: e2 studio Installation Confirmation and Extraction
 

Once the file extraction completes, a new pop-up will appear which will allow you to install the ISDE as a Quick or a Custom Installation. Select the Quick Installation unless you are an experienced user and have a specific need for a custom installation. Then click Next.

Quick_Install.PNG

Figure 4: Installation Selection

The default settings of the Installer are displayed. In most cases the default should be acceptable.

Install_Set_up.PNG

Figure 5: Installation Welcome Window

If the default location isn't acceptable, click on Change in the Welcome Window and an Installation Location window will open. Input the desired location and click OK.

Install_Location.PNG

Figure 6: Installation Location

Click Next. The Licensing Agreement will be displayed. Review the agreement and if it is acceptable, Check I Agree and Click Next.

Install_Agree.PNG

Figure 7: License Agreement

The installer will now go through the installation process and will install all the needed components in sequence. This included e2 studio, the GNU compiler, SSP and a variety of supporting elements. The installation begins with Visual C++ as seen below.  The progress bar indicates the amount of installation completed as well as the element currently being installed.

Install_VisualC.PNG

Figure 8: Installation progress and Status

At the end of the installation process, the installer show the installation Results as seen below. Check the boxes if you want to run the e2 studio based ISDE and/or view the SSP User Manual. Installation is complete!

Install_Results.PNG

Figure 9: Installation Results

Go to Section 3 to see what additional Resources are available to help you develop with the Synergy Platform.

2.2: Install the IAR EW for Synergy based ISDE

To install the IAR EW for Renesas Synergy based ISDE, open the IAR EW installer.  Click Yes on the Confirmation window. This will begin the Extraction Process..

IAR_Start.PNG

Extracting.PNG
Figure 10: Extracting Files
 
 

Once the file extraction completes, a new pop-up will appear which will allow you to install the ISDE as a Quick or a Custom Installation. Select the Quick Installation unless you are an experienced user and have a specific need for a custom installation. Then click Next.

IAR_Quick.PNG

Figure 11: Installation Selection

The default settings of the Installer are displayed in the Welcome window. In most cases the default should be acceptable.

IAR_Welcome.PNG

Figure 12: Installation Welcome Window

If the default location isn't acceptable, click on Change in the Welcome Window and an Installation Location window will open. Input the desired location and click OK.

IAR_Location.PNG

Figure 13: Installation Location

Click Next. The Licensing Agreement will be displayed. Review the agreement and if it is acceptable, check I Accept and then Click Next.

IAR_Agree.PNG

Figure 14: License Agreement

The installer will now go through the installation process and will install all the needed components in sequence. This included IAR EW for Renesas Synergy, SSP and a variety of supporting elements. The progress bar indicates the amount of installation completed as well as the element currently being installed.

IAR_Progress.PNG

Figure 15: Installation progress and Status

Toward the end of the installation process, the installer brings up the IAR installation Wizard. Click next.

IAR_Install1.PNG

Figure 16: IAR Installation Wizard

The Wizard displays the License Agreement. Review the agreement and if acceptable, Check I Accept and then Click Next.

IAR_Agree_EW.PNG

Figure 17: IAR EW for Renesas Synergy License Agreement

 

The Wizard will display the default installation location.

IAR_Location_EW.PNG

Figure 18: IAR EW for Renesas Synergy Installation Location

If needed, change the location by clicking the Change button. Click next.

The Wizard will display the selection for the Debug probe drivers. Click Next.

IAR_Probes.PNG 

Figure 19: Probes Selection

The Wizard will display the folder location. Accept the default and Click Next.

IAR_Folder.PNG

Figure 20: Selection for Installation Folder

The Wizard displays the ready screen.

IAR_Ready.PNG

Figure 21: IAR EW for Renesas Synergy Ready Screen

Click Install and the Wizard will display the progress bar.

IAR_Progress.PNG

Figure 22: Installation Progress

Once installation is complete the Finish Status window is displayed. Check the boxes if you want to run the IAR EW for Renesas Synergy based ISDE and/or view the release notes.

IAR_Finish.PNG

Figure 23: Installation Status Finish Screen

To complete the installation you will need to obtain a license file if you don't already have one from a previous installation. Follow the steps in the below article to obtain and load the needed license file.

How do I get a license file for the IAR EW for Renesas Synergy based ISDE.

 

Now, continue to Section 3 to see what additional Resources are available to help you develop with the Synergy Platform.

 

3: Additional Resources

Congratulations! You have now successfully installed the Synergy Platform. Here is a handy list of additional Synergy related resources available to speed your development projects:

  • Module Guides and Application Projects (Your primary source for detailed examples showing working code)
  • Solution Gallery (The complete collection of Synergy related software, tools, hardware, kits, partner projects, application projects and more!)
  • YouTube channel (Quick introductions to key Synergy capabilities)
  • Developer Examples (SSP 1.2.0)  (from Synergy Gallery- good test bench projects)
  • Renesas Academy  (six courses posted now – dozen more coming, excellent self-paced content)
  • IoT Community (information related to Synergy IoT targeted kits and projects)
  • Synergy Chat (from any Synergy page- a technical expert can answer quick questions on software, tools, kits, MCU's and more)
  • Knowledge base / FAQ (Extensive collection of Synergy related guides, FAQs, How to articles and helpful tips)
  • Renesas Rulz Synergy Forum (post questions and get answers to complex questions. You can even answer questions you know the answers to!)
  • Synergy Technical Bulletin Board (Frequent posts on key issues and work arounds. Subscribe for a periodic email notice on important topics)
  • Prof IoT Blog (Weekly post that help guide your development efforts and increase productivity)

4: Next Steps

Now that you have the ISDE installed you can begin development with the Synergy platform. Check out this article that shows how to best begin development with the Synergy platform. How to begin development with the Renesas Synergy Platform.