跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How much time, budget and manpower can users save by developing IoT applications with the Synergy Platform?

Latest Updated:10/04/2016

Question:

How much time will I save using the Synergy Platform for my IoT development project?

Answer:

The actual savings will vary with each project, but Renesas believes the Renesas Synergy Platform can provide significant savings in time, budget and manpower resources in the following areas:

  • Software - There is no need to purchase third party commercial RTOS, communication stacks (TCP/IP, USB), file systems, graphic user interfaces (GUI) and their associated development tools since they are included in the Renesas Synergy Platform.
  • Support – Customers don't need to purchase service or maintenance contracts since Renesas will warrantee the specification, provide regular feature upgrades and address all product questions through our global sales support organization.
  • Integration – As the Renesas Synergy Platform is fully-integrated as opposed to a set of separately sourced software and hardware components, Renesas is responsible for testing and qualifying the interoperability of the platform with our verified third-party suppliers against a written specification.  This will reduce the cost and time overhead required to manage relationships with different hardware and software component vendors.
  • 这篇文章对您有帮助吗?