跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How do I set a USB port for Device or Host designation within SSP?

Latest Updated:10/04/2016

Question:

How do I set a USB port, within SSP, for operation as a Device or Host?

Answer:

In SSP 1.1.0 there is a change to the use_ux_dcd_rx_initialize() API. The new version is use_ux_[h/d]cd_synergy_initialize() with the USB controller as argument. The controller will automatically be in host or device mode.