跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How do I keep SSP from overwriting header files I need to modify?

Latest Updated:10/02/2016

Question:

Sometimes I want to modify a header file that is automatically generated by SSP. Is there a way to keep SSP for overwriting these files?

Answer:

You can keep SSP from overwriting these files by giving them a file attribute of read only. Make changes sparingly however since it is difficult for Renesas to support changes you make to auto generated files.
Suitable Products
SSP