跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How do I download new application examples for the Synergy platform?

Latest Updated:09/19/2016

Question:

I notice there are a few application example designs (Project Templates) that come up in e2 studio after I have selected my target board. How do I add more of these application examples?

Answer:

Project Templates come up when you add a Synergy Project within the ISDE as seen below:

ProjectTemplates.png

 

You can find more Synergy designs, by importing them instead. You will find these Application Examples on the Renesas web site on the Tools and Kits page: 

https://www.renesas.com/en-us/products/synergy/tools-kits.html# 

Use the Documentation Tab, then check sample codes and then search to get a list of all the example designs. Simply import the Application Example as instructed in the associated Getting Started Guide downloaded with the project files.