跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How do I control the order of thread initialization in an SSP project?

Latest Updated:10/24/2016

Question:

How do I control the order of thread initialization in SSP?

Answer:

Threads are initialized in the order of priority. However you can fully control the initialization sequence via the following process:

1) Enable autostart for 1 thread only (set others to disabled)

2) Start other threads using tx_thread_resume().

3) You will need to create external linkage with the thread handle to make it visible from other threads (i.e. extern TX_THREAD gui_thread), as tx_thread_resume needs a pointer to the thread control structure in order to resume it.

A good example of how this is done is found in our GUIX Audio Player application note available on the Renesas web site- here

Suitable Products
SSP