跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How do I add a new pin configuration with a new structure in SSP 1.1. Alpha and e2 studio 5.x?

Latest Updated:10/02/2016

Question:

How do I add a new pin configuration with SSP 1.1 alpha and e2 studio 5.x?

Answer:

To add a new pin configuration with a new structure, you need to add a new pin configuration file.

The easiest way to do this:
- In the e2 studio Project Explorer, create a copy of the existing *.pincfg file and give it a unique name
- In the Pin Configurator, select the new pin configuration file you just created using the pull-down menu
- Tick the 'Generate Data' box and add a name for your data structure
- Modify the new pin configuration as required
- Generate project Content
- You will see that pin_data.c now includes both structures.

Notice that you will also get two CSV files in synergy_cfg\ssp_cfg\bsp\, one for each pin configuration.

Suitable Products
SSP 1.1x