跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How do I access registers on a Synergy MCU directly? Is there an API for that?

Latest Updated:10/18/2016

Question:

Is there an easy way to access registers on a Synergy MCU directly, with an API?

Answer:

You can access registers directly. For example, to access Ethernet register you would type in "R_ETHERC0->" and the smart completion feature in the ISDE will show suggestions for various registers to complete the code. Registers with a "-b" prefix are structures with access to specific bits.
Suitable Products
SSP