跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How can I Adjust the Autocomplete settings in e2 studio for editing my source files?

Last Updated: 04/25/2016

Question:

How do I adjust autocomplete options within e2 studio for edits to my code?

Answer:

You can adjust these options by edits to the preferences within e2 studio as shown in the example below:

Window > preferences > C/C++ > Editor > Templates > Comment (default multi-line comment)

If you are particularly concerned with the way comments are handled, and that asterisks always appear on newlines in comments,

you can also just type in your comments as regular text and then highlight the text and press Ctrl+Shift+/ to comment the text.

If you want to start the code block with a /* then hit enter, press backspace two times. Start writing your comment. Asterisks will no longer appear on newlines in that comment.