跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Do I need to run initialization for GUIX/LCD on the SK-S7G2 kit?

Latest Updated:12/08/2017

Question:

Is there any initialization needed when running GUIX/LCD on the SK-S7G2 kit?

Answer:

Yes, there is an initialization sequence needed. You can look at the Hello World application note to see what code is needed. This application note is available on the Tools and Kits page located here: https://www.renesas.com/produc...ols-kits.html. Select the Sample Program Tab. Expand the MPU/MCU Peripherals search filter and then click on Other Peripheral Function and select LCD. Click on Search and the Hello World example will come up in the results window as one of the top results.
Suitable Products
GUIX, SK-S7G2