跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Do I need a license from Microsoft if I use FileX FAT32/exFAT in a product I release to the market?

Latest Updated:09/15/2016

Question:

Do I need a license from Microsoft before I release a product to market that uses FileX FAT32 and/or exFAT?

Answer:

If you look on the Express Logic web site, at the below URL, you will see at the bottom of the page that they suggest you contact Microsoft for licensing information concerning Fat32 and exFAT support:

http://rtos.com/products/filex/