跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can I include special characters in my install or workspace paths for e2 studio and SSP?

Latest Updated:09/15/2016

Question:

Can I include special characters in the install path or workspace path for e2 studio and SSP? What happens if I do?

Answer:

If you put special characters in your install or workspace path e2 studio and SSP may not be able to find your project files. You may get errrors reported that it can't find include files for example. You should remove all spaces and non-standard characters from all your paths.