跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Where to find my target MCU part name in the list for M16C/Tiny series?

Latest Updated:09/04/2009

Question:

For M16C/Tiny series, I could not find my target MCU part name in the MCU list?

Answer:

On IO Wizard, the peripheral settings display for each MCU group are designed based on higher pin package device. Corresponding to the peripheral settings supported on IO Wizard, only higher pin package MCU devices are listed for user selection.

For M16C/tiny series :

  1. M16C/26A group - 48 pin package device part name are listed for selection. 42 pin package device part name are not available for selection.
  2. M16C/28 and 29 group - 80 pin package device part name are listed for selection. 64 pin package device part name are not available for selection.
Suitable Products
  • 这篇文章对您有帮助吗?