跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What kinds of evaluation tools for Renesas CAN MCUs do you have?

Latest Updated:10/29/2005

Question:

What kinds of evaluation tools for Renesas CAN MCUs do you have?

Answer:

The following is a main evaluation tool for Renesas CAN MCUs.

Development tool-

  • Hitachi ULSI Systems
    ・Micom Target System "Solution Engine"
  • VECTOR
    ・CAN Analyzer: CANalyzer
    ・CAN Oscilloscope: CANScope
    ・OSEK/VDX 2.0 compliant real-time multitasking operating system: osCAN etc.
  • Yokogawa Disital Computer Corporation
    ・CAN Flash Writer: C"arNET IMPRESS etc.

 

Suitable Products
R8C/22
R8C/23
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/1N