跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Regarding memory placement, is there a good method for the problem?

Latest Updated:12/01/2011

Question:

Regarding memory placement, I would like to define entities from the current C language, but entities not getting placed in the definition sequence.
Is there a good method for the problem?

Answer:

No.
If you want to specify placement, define entities in assembler and not C language, making the symbols names that start with "_" and declarat as public symbol.
For C, use external declarations removing the "_" from symbol name.
Suitable Products