跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Will my floppy disk be return after ROM mask processing is completed?

Latest Updated:09/15/2006

Question:

[QzROM, R8C/Tiny, M16C, 7900, 7770, 38000, 740/7450/7470, 7600, 7200, 4500, 720, OSD, ASSP] Will my floppy disk be returned to me after the ROM mask generating processing is completed?

Answer:

No, as a rule we do not return the floppy disk to the customer
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering