跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is data value of code and data flash memory after erasure in MCUs?

Latest Updated:12/20/2013

Question:

What is the data value of the code flash memory and data flash memory after erasure in MCUs of the RL78 family?

Answer:

The data value of the code flash memory and data flash memory after erasure is FFH.
Suitable Products
Flash Self Programming Libraries
Data Flash Libraries