跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is there a problem with a device if certain error as not defined show up?

Latest Updated:12/01/2011

Question:

In the SFRs of the MA1, DRC1 and SCR1, DRC3 and SCR3, DRC4 and SCR4, and DRC6 and SCR6 are set to the same address, respectively.
When compiled, a "Not Defined" error occurs for SCR1, SCR3, SCR4, and SCR6.
Is this a problem with the device file?

Answer:

Yes it is.
The current device file defines DRCx only and does not define SCRx.
This is the reason for this error.
Suitable Products