跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is it possible to create a LIB file with Project Manager?

Latest Updated:12/01/2011

Question:

I would like to create a LIB file with Project Manager, but is this possible?

Answer:

To make an object file into a LIB file, use the librarian provided in the assembler package.
To create a LIB file in Project Manager, set "Series Name" in the "Project Settings" dialog box to "xxxxx Series Library".
Various settings and execution vis-a-vis the librarian are possible from the Project Manager.
Suitable Products