跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is it possible to connect H-UDI with on-chip debugging emulator?

Latest Updated:06/28/2011

Question:

The section for the H-UDI is not found in your Hardware Manual. I wonder if it is possible to connect H-UDI with on-chip debugging emulator. If it is, I would like to request you to show a connection circuit example.

Answer:

It is possible to connect H-UDI with the on-chip debugging emulator(E10A-USB).
For more information on connecting with E10A-USB, please access to the web site for the E10A-USB and click the following items among the lists of documents to download.
“Super HTM Family E10A-USB Emulator Additional Document for User’s Manual,
Supplementary Information on using the SH7083, SH7084, SH7085 and SH7086”
“Super HTM Family E10A-USB Emulator Additional Document for User’s Manual,
Supplementary Information for using SH7146,and SH7149”
“Super HTM Family E10A-USB Emulator Additional Document for User’s Manual,
Supplementary Information on using SH7136 and SH7137”
“Super HTM Family E10A-USB Emulator Additional Document for User’s Manual,
Supplementary Information on using SH7125 and SH7124”

Click here to download the information on the E10A-USB.
E10A-USB Documents
http://www.renesas.com/products/tools/emulation_debugging/onchip_debuggers/e10ausb/Documentation.jsp
Suitable Products
SH7124, SH7125
SH7146, SH7149
SH7137
SH7136
SH7083, SH7084, SH7085, SH7086