跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is it OK if command prompt input is lower-case and part name upper-case?

Latest Updated:09/15/2006

Question:

I want to specify the command prompt input in lower-case letters and the part name in upper-case letters, using MM for the command type. It is acceptable to mix characters like this?

Answer:

MM will register the part name in the mask file in upper-case data. When the number is in the lower-case, MM will automatically convert it to upper-case letters and register it in the mask file. Upper-case letters will be registered as is. In other words, inputting the command prompt in lower case letters will not cause a problem, as the letters will be converted to the upper case automatically.
For more details, please refer to the MM User's Manual, "Process for Generating a Mask File: Part Name".
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering