跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

I would like to allocate multiple RAM section into the same memory

Latest Updated:09/10/2007

Question:

I would like to allocate multiple RAM section into the same memory.

Answer:

Please use the start command.

[Example]

optlnk test1.obj,test2.obj -start=PA,PB:PC/1000;

Allocate both PA and PC from No.1000. Allocate PB after PA.

Suitable Products
C/C++ Compiler Package for SuperH Family
C/C++ Compiler Package for H8SX, H8S, H8 Family