跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How to install PDG to PC not connected to the network?

Latest Updated:02/18/2013

Question:

How should I install the Peripheral Driver Generator to a PC that is not connected to the network?

Answer:

The Peripheral Driver Generator requires the following two software environments.
If these software packages have not been installed, the installer of the Peripheral Driver Generator obtains them from the network and starts installation. Therefore, install the following two software packages in advance when installing the Peripheral Driver Generator to a PC that is not connected to the network.

Suitable Products
Peripheral Driver Generator