跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How to generated source codes from IO Wizard into HEW if HEW is open?

Latest Updated:09/04/2009

Question:

Why is it that I cannot export the generated source codes from IO Wizard into HEW even when HEW is opened?

Answer:

You might have open HEW without opening any workspace. Please open an existing workspace and try again.
Suitable Products
  • 这篇文章对您有帮助吗?