跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How to deal with this error message "Data-file column exceed 255"?

Latest Updated:09/15/2006

Question:

I am getting the error message "Data-file column exceed 255". How should I deal with it?

Answer:

This error message is displayed when a column in the mask information file (extension .mmd) exceeds 255 characters. If the path to the hexadecimal data file is too long, shorten it so that the column of the mask information file is within 255 characters. For details concerning the Mask information file format, refer to MM User's Manual, Appendix C.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering