跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How to create a link file in a program executed by booting EPROM?

Latest Updated:12/01/2011

Question:

I would like to ask a question about how to create a link directive file.
Data is mapped at 0x800000, and then CONST is mapped at 0x70000.
I want the program to be executed by booting it from external EPROM, but it does not work normally.

Answer:

The address of CONST is lower than the address of data.
Such an arrangement is not allowed. Arrange them in address order (refer to 6.4 "Link Directive Format" in the Operation manual).
Suitable Products