跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How can a library be created?

Latest Updated:12/01/2011

Question:

I would like to put some functions into a library.
How can a library be created? (I cannot find appropriate options for creating a library.)

Answer:

Library creation is provided as an archiver function not as option specification.
The actual library creation procedures are described in Chapter 9 "Archiver" in the Operation user's manual.
Suitable Products