跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How can I specify addresses in EEPROM Pack01 and EEPROM Pack02?

Latest Updated:10/24/2014

Question:

How can I specify addresses to read data written by the given library (one of the followings) in a product of the RL78 family ?

  • EEPROM Emulation Library Pack01
  • EEPROM Emulation Library Pack02

Answer:

EEPROM emulation libraries Pack01 and Pack02 for the RL78 family do not have a function to read data at specified addresses.
However, data can be read in one-byte units by a CPU instruction.
In addition, if you are using the Data Flash Library Type04 for the RL78 family rather than an EEPROM Emulation Library, this library is capable of reading data from specified bytes.
Suitable Products
Data Flash Libraries