跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How can I know ROM capacity ?

Latest Updated:09/10/2007

Question:

How can I know ROM capacity ?

Answer:

In order to check the ROM capacity in the user program, a linkage map list file(*.map) can be used. There is the method of computing the sum of the section size applicable to ROM.Make the following setting before build in order to output the linkage map list file.

HEW3 -> Option(O) -> Select "H8S,H8/300 Standard Toolchain"

-> Select an Optimizing Linkage Editor Tab, and select a "List" as Category(Y). Then check for [Generate list file(G)], and click [Enable all(E)].

Suitable Products
C/C++ Compiler Package for SuperH Family
C/C++ Compiler Package for H8SX, H8S, H8 Family