跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How are load module files divided to output in building?

Latest Updated:11/19/2014

Question:

I'm using the SH compiler. How are load module files divided and output in building?

Answer:

Load module files can be divided into output ranges (addresses or sections) by using an option of the optimizing linkage editor.

Please specify the option when building, follow these steps:

  1. Select the High-performance Embedded Workshop menu [Build] -> [SuperH RISC engine Standard Toolchain]
  2. Select the [Link/Library] tab, and then select the following settings.
    [Category]: Output
    [Show entries for]: Divide output files
  3. Select the [Divide output files] checkbox.
  4. Specify the file name and the output range (address or section) after division.

For details on the -output option, refer to the following section here.

  • SuperH C/C++ Compiler Package V.9.04 User's Manual
    Section 4 Optimizing Linkage Editor Options
    4.2.2 Output Options
    -output

When the following types are specified as [Type of output file] in the High-performance Embedded Workshop, divided multiple load module files (*.mot, *.hex, or *.bin) and an *.abs file are generated.

  • S type via absolute
  • HEX via absolute
  • Binary via absolute
Suitable Products
C/C++ Compiler Package for SuperH Family