跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Do I have to describe the jump instruction in assembly language?

Latest Updated:02/01/2009

Question:

Do I have to describe the jump instruction to the user handler routine in assembly language?

Answer:

Yes, you have to describe them in assembly language.

<For referencce>
 Flash Memory Self-Programing Library
  V850 Microcontrollers Type 01 [Ver.5.00]
   U18208EJ3V0UM00(3rd edition)
    2.11.4 Interrupt servicing in flash environment (Customer Method)

  V850 Microcontrollers Type 03 [Ver.2.00]
   U18211EJ2V0UM00(2nd edition)
    2.11.1 Interrupt servicing in flash environment
Suitable Products
V850 Family